Technical FAQs

Ask a Question

What is the difference in a ATV61 and ATV71 drive?

Issue:
Constant and Variable torque application requirements

Product Line:
All ATV61/71 drives

Environment:
ATV61/71 drives

Cause:
What is the difference in a ATV61 and ATV71 drive?

Resolution:
ATV61 AC Drive Products for Centrifugal Pumps and Fans (for Variable Torque Applications).
ATV71 AC Drive Products for Applications Such As: Conveyors, Mixers, Extruders and Material Handling (for Constant Torque Applications).
Was this helpful?
What can we do to improve the information ?