Technical FAQs

Ask a Question

HOA switch working backwards after ATV58 was replaced with ATV61

Issue:
After replacing the ATV58 with an ATV61 the HOA is working backwards.

Product Line:
EconoFlex 58

Environment:
All

Cause:
Reference analog input programming  need to be changed on the new ATV61 drive.

Resolution:
New ATV61 needs to be programmed.
  • Menu 1.6 Command menu
  • Ref 1 = AI2
  • Ref 1 B switching = LI3
  • Ref 1 B channel is AI1
  • Logic input LI3 is low for auto and high for hand.

Reference the ATV61 Programming manual.

 
Was this helpful?
What can we do to improve the information ?