Technical FAQs

Ask a Question

What is the highest HP size in an NEMA 12 for the M-Flex enclosed drives?

Issue:
Max highest HP size in an NEMA 12 for the M-Flex enclosed drives

Product Line:
M-flex enclosed

Environment:
All

Cause:
Specifications

Resolution:

The M-flex with ATV61 VT applications is available in NEMA 12 up to and including 100HP 480vac only
The M-flex with ATV71 CT applications is available in NEMA12 up to and including 75HP 480vac only

ATV71 CT 230vac  max HP size is 40HP
ATV61 VT 230vac max HP size is 50HP

Reference the M-Flex enclosed instruction manual 30072-451-52.
 
Was this helpful?
What can we do to improve the information ?