Technical FAQs

Ask a Question

What line reactor is recommended for a ATV61HD45M3X in an 240V 30hp single phase application?

Issue:
What line reactor is recommended for a ATV61HD45M3X in an 240V 30hp single phase application?

Product Line:
Altivar 61/ 71  ATV61 ATV71

Environment: 
ATV61HD45M3X  ATV71HD45M3X

Cause:
Application requires line reactors
 
Resolution:
Part number for a 5% line reactor is  RL20003
 
Was this helpful?
What can we do to improve the information ?