Technical FAQs

Ask a Question

Customer is needing a hands off auto switch and two micro switches, ZBE203/5 and needs part number for hand off auto?

Customer needs the part numbers for the HOA (Hand Off Auto) switch 
Product Line:
 E-Flex 8839
 All models
Hand-Off-Auto Selector Switch
ZB5AD3 Three-position selector switch
ZB5AZ009 mounting collar
ZBE205 Additional contact block (1 N.O., 1 N.C.)
(2) ZBE102 Additional contact block (1 N.C.)
ZBE203 Additional contact block (2 N.O.)
ZBZ32 Legend plate holder
Was this helpful?
What can we do to improve the information ?