Technical FAQs

Ask a Question

What is the part number for the bracket support for a Model 5 MCC mid shelf?

Without buying the entire mid shelf assembly (80450-830-50) , can the mounting Feet (Brackets) be ordered separately?

Product Line:
Model 5 Motor Control Centers (MCC)

Replacement mid shelf parts for Model 5 MCC

The loss, or non shipment of of brackets as well as replacement

The Bracket (Mounting Foot) for the Mid shelf assembly is part number 80450-623-01

Was this helpful?
What can we do to improve the information ?