Technical FAQs

Ask a Question

Customer has an ATV71HD18N4 and has OLF

Issue: 
Getting an OLF fault on a  ATV71 drive.

Product Line:
Altivar ATV71 and ATV61

Environment: 
All

Cause: 
Motor is pulling to much current

Resolution: 
[Motor overload] • Triggered by excessive motor current.  Check motor  load. Check motor nameplate settings in the drive. Also check current limitation settings.  
Verify the motor current is balanced in all three legs, and not exceeding the motor FLA.  

Was this helpful?
What can we do to improve the information ?