Technical FAQs

Ask a Question

What are the dimensional differences between the S-Flex drives with and without Bypass?

Issue:
What are the dimensional differences between the S-Flex drives with and without Bypass?
Product Line:
All S-Flex, SFD drives. 
Environment:
All models, all serial numbers
Cause:
Needs dimensions
Resolution:
The S-Flex is a standard drive.  The enclosure dimensions are the same for both Bypass and Without Bypass. 
Was this helpful?
What can we do to improve the information ?