Technical FAQs

Ask a Question

Can the ATV71 ATV61 be configured for lead lag applications with 2 drives using PID control?

Issue
Lead / Lag application requirement using PID

Product Line: 
Altivar61 Altivar71 ATV61 ATV71 
 
Environment: 
All

Cause:
Application requirement.

Resolution
Unable to comply with this type of configuration, no available options.


 
Was this helpful?
What can we do to improve the information ?