Technical FAQs

Ask a Question

What are the recommended torque specifications on the NSYTRV42 terminal block?

Issue:
What are the recommended torque specifications on the NSYTRV42 terminal block?

Product Line:
IEC Terminal Blocks

Environment:
Typical installation and application

Cause:
Assembly/installation, wiring

Resolution:
The recommended torque specifications are:
0.6-0.8 Nm (5.31-7.08 inch-lbs)

 

Was this helpful?
What can we do to improve the information ?