Technical FAQs

Ask a Question

Where can dimensions for a 8930IFD Field Drive be found?

Issue:
Need dimensions for a 8930IFD Field Drive

Product Line:
ATV61 ATV71

Environment:
All

Cause:
No documentation

Resolution:
See Instruction Bulletin number 30072-454-01 for dimensions on Class 8930, type IFD enclosed drives. 
Was this helpful?
What can we do to improve the information ?