Technical FAQs

Ask a Question

What are the dimensions of the ATV61HD22N4?

Issue:
What is the overall dimensions for the ATV61HD22N4?

Product Line:
Altivar ATV61

Environment:
Part number specific

Cause:
None

Resolution:
Width - 9.45"
Height - 16.54"
Depth - 9.29", includes graphic keypad and no option boards.
Weight is  66.14 lbs

 

Was this helpful?
What can we do to improve the information ?