Technical FAQs

Ask a Question

How to properly connect a Square D Low voltage transformer with voltage codes S1F or S3H, rated for 240 x 480 - 120/240 volts or 240V?

Issue:
How to properly connect a Square D Low voltage transformer with voltage codes S1F or S3H, rated for 240 x 480 - 120/240 volts or 240v?

Product Line:
LV Transformers

Environment:
Applies to Single Phase Transformers with 480V x 240V primaries and 240/120V secondaries ONLY.

Cause:
Wording:  "V On Lines"  and  "Connect"  on Epoxy Resin Encapsulated Transformer nameplates.

Resolution:
Connections depend on your application.

Primary:
For 480V connect H2 and H3 together and apply primary 480V lines to H1 and H4
For 240V connect H1 and H3 together and connect H2 and H4 together, then apply 240V lines to H1 and H4

Secondary:
For 120/240 Volt 3-wire: Connect X2 and X3 together and bond to equipment ground and building ground. 240V outputs are X1 and X4, neutral is the X2/X3 connection
For 120 Volt 2-wire: Connect X2 and X4 together and bond to equipment ground and building ground. Connect X1 and X3 together. 120V hot line is the X1/ X3 connection, neutral is the X2/X4
connection
For 240V connect X2 and X3 together then connect the 240V load wires to X1 and X4.

 
Was this helpful?
What can we do to improve the information ?