Technical FAQs

Ask a Question

What is the Main Lug wire range for the UHTRS213B individual meter socket?

Issue: 
Main lug wire range. 
 
Product Line: 

Individual Meter Sockets
 
Environment:
Main Lugs size 
 
Cause: 
Determining the main wire size to use.
 
Resolution:
The UHTRS213B will accept (1) #8 - 350kcmil Al/Cu wire for the Main Line, Load and Neutral and (1) #14 - #2 AWG Al/Cu wire for the Ground.
Was this helpful?
What can we do to improve the information ?