Technical FAQs

Ask a Question

What is the combination suffix for 1143, 24Vac under voltage release (UVR) in the left pole and 1212, 1a1b auxiliary contact in the right pole?

ISSUE
What is the combination suffix for 1143, 24Vac under voltage release (UVR) in the left pole and 1212, 1a1b auxiliary contact in the right pole? 

PRODUCT LINE
Black Legacy breaker frames like F, K, L, M, N, P

ENVIRONMENT


CAUSE
To identify the breaker accessory options.

RESOLUTION

Combination suffix 1612.

 
Was this helpful?
What can we do to improve the information ?