Technical FAQs

Ask a Question

What is the replacement for the XBTNREQ3866G Altivar Message Display Center?

Issue:
Inoperative XBTNREQ3866G Altivar Message Display Center

Product Line:
Altivar 58  ATV58

Environment:
All models, All series

Cause:
Need XBTNREQ3866G or replacement.

Resolution:
There is no direct replacement for the Altivar Message Display Center.
If the display is being used on an ATV58 drive try using an ATV58 keypad display. (part number VW3A58101U)  This display, however, only displays three characters at a time.


 
Was this helpful?
What can we do to improve the information ?