Technical FAQs

Ask a Question

What is the part number for the green terminal block inside the E-Flex enclosed drives?

Issue: 
What is the part number for the green terminal block inside the E-Flex enclosed drives?

Product line:  
Altivar ATV61 E-Flex

Environment: 
All models, all serial numbers

Cause:
Replacement terminal block part number

Resolution:
The replacement terminal block part number is 25410-00200.  This part has to be forced to order through the Seneca plant.
Was this helpful?
What can we do to improve the information ?