Technical FAQs

Ask a Question

What is the part number for the power converter inside the E-Flex 8839 EFDDG4Y?

Issue:
What is the power converter part number for an 8839 EFDDG4Y enclosed drive?

Product Line:
E-flex enclosed products only

Environment:
All

Cause:
Replacement drive inside the enclosure.

Resolution:
ATV61H075N4  Please note this drives power ID will need to be changed in the programming  from IP20 to IP00 so that the HP size can be up sized.
To change the power ID you must be in expert mode, got menu 1.4 and find power ID  set to IP00 enter.  Drive will reset back to factory default which you will need to reprogram the drive.
Note: for other HP and voltage sizes look at the E-Flex install manual 30072-451-51D,
 
Was this helpful?
What can we do to improve the information ?