Technical FAQs

Ask a Question

Number of Serial RS232 ports on SLC5500PC PCI

Attempting to connected to the SLC5500PC PCI with Powerlink and toolkit at the same time and when doing so Powerlink does not see the state change of the CBus groups.

Note: As of March 1, 2015 all US Lighting Control products (EXCEPT Powerlink and MVP panels) will enter their obsolescence phase and will no longer be purchasable for new orders. Management of the Prosumer Business has made a strategic decision to stop the Lighting Control initiative and concentrate our effort in new businesses with higher growth potential – Connected Home, Building Control in small buildings, and Electric Vehicle solutions.

Product Line:
Clipsal CBus SLC5500PC, Powerlink
Connected to Toolkit and LCS at the same time.
SLC5500PC has two RS232 RJ45 plugs available on the top of the device labeled RS232 and one DB9 port on the front of the device. However all share one internal serial port.
Disconnect toolkit before testing if the Cbus network is communicating with the Powerlink panel through the RS232 port.
Was this helpful?
What can we do to improve the information ?