Technical FAQs

Ask a Question

What is the replacement for the seal kit catalog number 29375 used on the DJM Circuit breaker?


ISSUE: The seal kit catalog number 29375 for DJM frame breakers has been obsoleted since the DJM breakers are obsolete. What is the direct replacement?  

PRODUCT:  LINE DJM Breakers   

ENVIRONMENT:  Applies to DJM breakers that used the seal kit catalog number 29375.  

CAUSE: Seal kit catalog number 29375 is now obsolete and no longer available.  

RESOLUTION: The replacement seal kit for catalog number 29375 is catalog number  S29375.

Was this helpful?
What can we do to improve the information ?