Technical FAQs

Ask a Question

Does Schneider Electric / Square D offer IEC rated Disconnects?

Issue:
Does Square D by Schneider Electric offer IEC rated Disconnects?
 
Product Line: 
IEC Rated Disconnects

Environment:
Applies to all IEC rated Disconnects.

Cause:
Selection of a disconnect that is IEC rated

Resolution:  
Square D does offer some Disconnects that are IEC rated depending on the applicaton and type required. However, the General Duty, Heavy Duty and Double Throw Safety Switches are NOT IEC rated disconnects. Customers would need to contact Schneider Electric (888) 778-2733, Option 1 with their specifications for further information and to determine if there is a IEC rated disconnect to meet their needs.
Was this helpful?
What can we do to improve the information ?