Technical FAQs

Ask a Question

What is the part number for the ATV61HD55N4 motor current sensors?

Issue:
What is the part number for the ATV61HD55N4 motor current sensors?

Product line:
Altivar ATV61

Environment: 
All models, all serial numbers 
Cause:  
Replacement parts 
Resolution: 
The part number for the current sensor is VY1A1104. However, it is only available through Field Services.
Was this helpful?
What can we do to improve the information ?