Technical FAQs

Ask a Question

How do you wire a remote potentiometer to an ATV12 drive?

Issue:  How do you wire a remote potentiometer to an ATV12 drive?

Product line:   Altivar ATV12 
Environment:  All models, all serial numbers 
Cause:  Field wiring a remote pot into the ATV12 drive.     
Resolution: Wiring as follows:  wiper of he pot wires to AI1, high side of the pot wires  to +5 vdc and low side of pot wires to com
Was this helpful?
What can we do to improve the information ?