Technical FAQs

Ask a Question

Product selection for a ATV61 575vac 100HP drive.

Issue:
Product selection for a 575vac 100HP drive.

Product line:
Altivar ATV61

Environment:
All models, all serial numbers 

Cause:
ATV61 Product selection for a 575vac 100hp open type drive.   
 
Resolution:
VT fan and pump applications only =ATV61HD90Y + optional line reactor RL10003  
CT conveyors, mixers etc = ATV71HD90Y + optional line reactor RL10003
Was this helpful?
What can we do to improve the information ?