Technical FAQs

Ask a Question

What is the maximum number of contact blocks that can be mounted to a 9001SK Push Button?

Issue:
How many contact blocks can be mounted to a maintained 9001SK Push Button?

Product Line:
Operator Interface Push buttons 30mm

Environment:
1,3R, 4, 4X, 12
IP54, 55, 65

Cause:
Installation and Configuration

Resolution:
Maximum is 4 contacts blocks (4) 9001KA1
Was this helpful?
What can we do to improve the information ?