Technical FAQs

Ask a Question

ATV212 with Metasys N2, Can the KW consumption be reset?

Issue:
ATV212 with Metasys N2, Can the KW consumption be reset?
Product line:
Altivar ATV212
Environment:
All models, all serial numbers
Cause:
Need to reset energy counter
Resolution:
With Metasys, you are using a BACnet protocol. By writing a value in AV#8, the energy counter should be reset.

Refer to the ATV212 Metasys N2 manual ATV212_Metasys manual_N2_EN_S1A53846_01

Was this helpful?
What can we do to improve the information ?