Technical FAQs

Ask a Question

What is the Max Line current for ATV61HD37M3X at 240 Vac?

Issue:
What is the max Line current for ATV61HD37M3X at 240 Vac?
Product line:
Altivar ATV61
Environment:
ATV61HD37M3X
Cause:
Basic feature for the ATV61 drive.
Resolution:
Max is 127 amps.

Refer to the ATV61 Catalog DIA2ED2050905EN
Was this helpful?
What can we do to improve the information ?