Technical FAQs

Ask a Question

What are the component parts for a 9001KXRG35RWG?

Issue:
What are the component parts for a 9001KXRG35RWG?

Product Line:
Operator Interface Push Buttons

Environment:
NEMA 1, 3R 4 and 12
IP55 and IP66

Cause:
Components are not listed in the product catalog

Resolution:
The component parts for 9001KXRG35RWG are:
  • 9001KXRG
  • 9001KM35
  • 9001kXAW4
  • 9001KXAR3
  • 9001KXAG3.
Was this helpful?
What can we do to improve the information ?