Technical FAQs

Ask a Question

What is the screw size for the cover on a 9001TY1?

Issue:
What is the screw size for the cover on a 9001TY1?

Product Line:
Control stations

Environment:
NEMA 1, 4, 12

Cause:
Not specified in the product catalog

Resolution:
The screw size is 10-24 x 1 3/8
Was this helpful?
What can we do to improve the information ?