Technical FAQs

Ask a Question

What is the mounting kit part number when converting an ATV58HD64N4XZ over to an ATV61HD55N4?

Issue:
What is the mounting kit part number when converting an ATV58HD64N4XZ over to an ATV61HD55N4?

Product line:
Altivar ATV58 and ATV61

Environment:
All models, all serial numbers

Cause:
Needs a mounting plant to match up the mounting holes after swapping out an ATV58HD64N4XZ with an ATV61HD55N4 drive.   

Resolution:
Mounting plate kit part number is VW3A9312


 
Was this helpful?
What can we do to improve the information ?