Technical FAQs

Ask a Question

What is the replacement cover part number for HOM42M225RB, Series S01, S02 or S03 Load Center?

ISSUE:
Repair Parts

PRODUCT LINE:
Homeline Load Centers

ENVIRONMENT:
Applies to HOM42M225RB, Series S01, S02 or S03.

CAUSE:
Maintenance

RESOLUTION:
The part number for a replacement door (cover) for the HOM42M225RB, Series S01, S02 or S03 is 40563-172-50. The cover would include the hinges. If needed, the replacement cover mounting screws are part number 21422-17101 (2 required).
Was this helpful?
What can we do to improve the information ?