Technical FAQs

Ask a Question

Is there a listing or data /cut sheet that shows the drive dissipated heat in the 8930 IFD field drives?

Issue: 
Is there a listing or data /cut sheet that shows the drive dissipated heat in the 8930 IFD field drives?

Product line: 
Altivar ATV61 ATV71 Field Drives

Environment: 
Al models, all serial numbers

Cause: 
What is the dissipated heat loss in the Field Drives?    

Resolution:  
We never did a chart like this for Field Drive. Being outdoor Type 3R units, the manual committee believed this chart was not necessary. For a rough estimate, Table 38 of the Field Drive manual gives the drive in each unit. I would take the ATV61 drive Installation manual heat loss data (power loss in control section + power loss in power section) and multiply by 1.5 to account for all the other components. 

Was this helpful?
What can we do to improve the information ?