Technical FAQs

Ask a Question

What is the part number for a line reactor for a 50hp 3 phase 230V drive?

Issue: 
What is the part number for a 5% line reactor for a 50hp 3 phase 230V drive?
Product line: 
Altivar All

Environment: 
All models, all serial numbers 
Cause: 
Basic Line or Load reactor for a 50HP 230VAC drive.     
Resolution:
RL13002= Open type line or load reactor
RL13012= NEMA 1 enclosed line or load reactor
Both reactors are 5%
Was this helpful?
What can we do to improve the information ?