Technical FAQs

Ask a Question

What material are the L100 levers made from?

ISSUE

What material are the L100 levers made from?

PRODUCT LINE

Limit Switches

ENVIRONMENT

This applies to all L100, and L300  products.

CAUSE

Compatibility of product with the application is in question.

RESOLUTION

Most are machined aluminum.  See the 9007 Mill and Foundry catalog for a complete listing.

Was this helpful?
What can we do to improve the information ?