Technical FAQs

Ask a Question

What is the part number for the generator interlock kit for HOM40M200C series S03?

ISSUE:
What is the part number for the generator interlock kit for HOM40M200C series S03?

PRODUCT LINE:
HOMELINE Load Centers

ENVIRONMENT:
Need to add a generator interlock kit to allow for backfeeding a generator source into the load center.

CAUSE:
Need for co-generation of power to the load center from a generator.

RESOLUTION:
The generator interlock kit for a HOM40M200C, Series S03, is HOMCGK2 or HOMCGK2C. The only difference between the HOMCGK2 and HOMCGK2C is the packaging.
Was this helpful?
What can we do to improve the information ?