Technical FAQs

Ask a Question

Can the PID feedback signal be replicated to another drive?

Issue: Customer wants the analog signal to operate two drives from one source.

Product line: Altivar 61, E-flex

Environment: All models, all serial numbers 

Cause: One PID signal to operate two drives. 

Resolution:

Under Drive Menu > Inputs/Outputs Configuration > AO1 Configuration > AO1 assignment, change this parameter to PID feedback.  Use the AO1 and COM terminals to feed the reference signal into the next drive. 
Was this helpful?
What can we do to improve the information ?