Technical FAQs

Ask a Question

Is the S-Flex Life Safety Certified?

Issue:
Is the S-Flex Life Safety Certified?
Product line:
S-Flex ATV212 ATV21
Environment:
All models, all serial numbers
Cause:
Certification needed
Resolution:
S-Flex hasn't been evaluated to NFPA 101, and after review of the document, I'm not convinced that specific equipment should be. The document "Life Safety Code" generally deals with methods and techniques of building construction and management. S-Flex product could be integrated into such a system for smoke purge (for example) and should be part of a maintenance and check of emergency systems as advised in NFPA 101. It is also my opinion that NFPA 70 is the applicable specification for the drives and 101 is applied to the control system.
Was this helpful?
What can we do to improve the information ?