Technical FAQs

Ask a Question

How can I get an indication that the drive is in Auto mode on the HOA selector switch?

Issue:   Customer would like indication to confirm the selector switch is in Auto mode. 

Product line: E-Flex

Environment: All models, all serial numbers 

Cause: None

Resolution:

Install a normally open contact on Auto side of the Hand-Off-Auto selector switch on the E-flex enclosure door.  When the switch is in Auto, the contact closes indicating the switch is in auto.
Was this helpful?
What can we do to improve the information ?