Technical FAQs

Ask a Question

Enabling NLD function for a ATV61 drive

Issue: Enabling NLD function for a ATV61 drive

Product Line: ATV61

Environment: ALL ATV61 Drives

Cause:  Needs the NLD feature  for the ATV61 drive?

Resolution: The ATV61 has this feature in Menu 1.4 , under the Motor Control Type, select energy Savings ( NLD). The NOLD (no load) function: Reduces the voltage to the motor when selected for variable torque loads. A constant volts/Hz ratio is maintained during acceleration. The output voltage will then automatically adjust to meet the torque requirement of the load
Was this helpful?
What can we do to improve the information ?