Technical FAQs

Ask a Question

Some of the ATV31 drives have an A on the end of the part number. What does the A mean?

Issue:
Need local controls.

Product Line:
Altivar 31 ATV31

Environment:
All

Cause:
Drive part number omits the A suffix.

Resolution:
The ATV***31A has the start/stop button, run button, and a potentiometer on the front of the drive. The ATV***31 without the "A" at the end of the part number does not have the start/stop, run, and potentiometer on the front of the drive.
Was this helpful?
What can we do to improve the information ?