Technical FAQs

Ask a Question

Does the start button remain depressed after the reset button is pushed on a 2510 M manual starter?

ISSUE
Does the start button remain depressed after the reset button is pushed on a 2510 M type manual starter?

PRODUCT LINE
Manual Starters

ENVIRONMENT 
2510

CAUSE
Operation and product features

RESOLUTION
When the reset button is pressed after a thermal overload, the start button returns to the extended position.
Was this helpful?
What can we do to improve the information ?