Technical FAQs

Ask a Question

ATV312: Can the program be changed while the drive is running?

Issue:
ATV312: Can the program be changed while the drive is running?

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
Sometimes parameters seem to be locked out from changing values.

Resolution:
Most parameters cannot be changed when there is an active run command.  However, some can be adjusted while the motor is running. All parameters can be viewed either way.
See the programming manual, document BBV46385:
http://www.schneider-electric.us/en/download/document/BBV46385/
Was this helpful?
What can we do to improve the information ?