Technical FAQs

Ask a Question

What is the catalog number for a ``sealing kit`` for use with the Masterpact NW and Masterpact NT breakers?

Issue:
What is the catalog number for a ``sealing kit`` for use with the Masterpact NW and Masterpact NT breakers?

Product Line:
Masterpact, Powerpact, Micrologic

Environment:
Products sold in North America

Cause:
Need to seal the trip unit after the levels are set.

Resolution:
Sealing Accessory # MICROTUSEAL can be used on the Masterpact NW and Masterpact NT breakers.


CTA-ID : 2063282
Was this helpful?
What can we do to improve the information ?