Technical FAQs

Ask a Question

What are the restrictions on using Powerpact P frame lug CU250P1K?

Application requirements for this lug are:
+ Circuit Breaker: PowerPact PJ only
+ Mounting: I-Line or Unit Mount
+ Micrologic Trip Unit
+ Sensor Plug: 250 A
+ Long-Time Setting: 100, 110, 125, or 150 A
+ Instantaneous Setting: Not OFF
+ Trip Unit: Sealed after setting with kit no. MICROTUSEAL
+ Cable Size: 1 or 1/0 AWG, CU
+ Load Wire Length: 25 ft. Minimum


CTA-ID : 2063284
Was this helpful?
What can we do to improve the information ?