Technical FAQs

Ask a Question

What are the dimensions for a XALD01H7?

Issue:
What are the dimensions for a XALD01H7?

Product Line:
22mm control station enclosure

Environment:
XALD

Cause:
Product features

Resolution:
The dimensions for the XALD01H7 are 2.68" H x 2.68" W x 2.09"D. These dimensions can be found in catalog 9001CT1104 or 9001CT0001.
Was this helpful?
What can we do to improve the information ?