Technical FAQs

Ask a Question

When should the motor control type be Sync. mot.?

Issue:
When should the motor control type "Sync. mot." be used?

Product Line:
ATV61 Altivar 61

Environment:
All

Cause:
Application requirements.

Resolution:
Sync. mot. type is used when synchronous permanent magnet motors with sinusoidal electromotive force (EMF) only are used.  Choosing this parameter enables Synchronous programming parameters. 
Was this helpful?
What can we do to improve the information ?