Technical FAQs

Ask a Question

ATV312 -How can you access the drive stop and run buttons on the drive with the door closed?

Issue:
How can you access the drive stop and run buttons on the drive with the door closed?

Product Line:
ATV312  Altivar 312

Environment:
All

Cause:
Require local control access.

Resolution:
You will be able to access the buttons on the drive while the drive door is closed if you pop out the plastic covers.
To pop out the plastic covers: Open the door from the front of the drive, look at the back side of the door, you will see 2 round molded pieces of plastic (where the cut out is on the front). Simply punch on these with (on the back side of the door), and they will pop out and be pushed out through the front. Once you have them removed, close the door, and you will then, be able to access the buttons on the drive with the door closed.
Was this helpful?
What can we do to improve the information ?