Technical FAQs

Ask a Question

Are the Altivar 61 and Altivar 71 drives equipped with a real time clock?

Issue:
Request for a timestamp

Product Line:
ATV61 ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
The Altivar 61 and Altivar 71 drives do not have a realtime clock so the timestamp function is not available.  In order to add a timestamp function, a Controller Inside Card (VW3A3501) or an IMC card (VW3A3521SO) will need to be installed.

 

Was this helpful?
What can we do to improve the information ?