Technical FAQs

Ask a Question

What is the dissipated power for ATV61HU30N4?

Issue:
Need to determine if additional cooling needs to be provided for ATV61HU30N4

Product Line:
ATV61

Environment:

All models and serial numbers

Cause:
None

Resolution:

Dissipated power for an ATV61HU30N4 drive with flange mounting is 135W and without is 740W in Nema 1 enlcosure.

 

Was this helpful?
What can we do to improve the information ?