Technical FAQs

Ask a Question

ATV61 drive trips on External fault due to momentary loss of input. Is there a way to program a time delay on a logic input that is programmed for External fault?

A Logic input has a built-in Time delay that is adjustable from 0-200 milliseconds. Factory default is 0 seconds. Need to go to Input/Output Configure menu and then to LIx configuration. Go to LIx On Delay and adjust the time as necessary.
Was this helpful?
What can we do to improve the information ?